13.1.1 File Menu
This section lists the menu items in the File menu.
For keyboard shortcuts of some of these menu items, see .
| Command | Action |
|---|---|
| New Project | Creates a new project with the New Project wizard. |
| New File | Creates a new file with the New File wizard. |
| Open Project | Opens an existing project. |
| Open Recent Project | Displays a
list of all recently-opened projects for selection. This list can be cleared by deleting the file /config/Preferences/org/netbeans/modules/projectui.properties under the User directory (where the path may be found under ). |
| Import | Imports one
of the following:
|
| Close Project | Closes the current project. |
| Close Other Projects | Closes all projects except for the main project. |
| Close All Projects | Closes all open projects. |
| Open File | Opens an existing file. |
| Open Recent File | Displays a list of all recently-opened files for selection. |
| Project Group | Associates the current project with a group. |
| Project Properties | Opens the Project Properties window. |
| Save | Saves the current file. |
| Save As | Saves the current file under a new path and/or name. |
| Save All | Saves all open files. If the Compile on Save feature is selected, this will also compile/build project files. |
| Page Setup | Sets up the page for printing. |
| Shows print preview of current file and allows printing. | |
| Print to HTML | Prints the current file to a new file in HTML format. |
| Exit | Quits MPLAB X IDE. |