5.11.3 Insert unprotected checksum in user ID memory
If it is supported by the device (not grayed out), click the check box to use the checksum number that was generated by the build as the user ID.
For the PIC32 family of devices, the checksum is dependent on the USER ID. Therefore, this feature is not supported under PIC32 devices.