4.6 Examining MCC Generated Files
Expand the project tree to see project files in MCC Generated Files folders. This means that the project was generated using the MPLAB Code Configurator, or MCC.
To see the MCC configuration that generated these files, you can install the MCC plugin by going to , checking MPLAB Code Configurator and clicking Install.
Note: You will need to restart.
Click the MCC icon
that is now on the toolbar to launch MCC. The
configuration information shown is from the project MyConfig.m3
file. To close MCC, click the icon again.