4.6.8.12.1 FP Status Access
The msws and lsws of the FSR are implemented as 16-bit registers which can be independently read
and written by the CPU and FPU. This is intended to prevent structural hazards arising
between
FTST/FCPS/FCPQ/FBcc
instructions (that access the FSR msw) and all other instructions that could affect the
exception status (located in the FSR lsw). Hazards are not expected to exist between
FTST and FCPS/FCPQ
instructions.
The FCPS/FCPQ/FTST status located in msw of the FSR (FSRH) can be read and stacked by the
PUSHCR instruction while the lsw of the FSR is written (or blocked
to be written). The msws and lsws of the FSR are otherwise concatenated into a single
32-bit value (FSR) for read/write by the MOVCRW/MOVWCR
and PUSHCR/POPCR instructions.
In addition, the FAND and FIOR instructions operate with a
16-bit literal and can be used to set or clear the bit in the FCR or lsw of the FSR or
FEAR. When the FSR is referenced in these ops, users can manipulate the FPU exception
status, but access to the FCPS/FCPQ/FTST status in FSRH is not possible. This choice
assumes that the need to modify FTST/FCPS/FCPQ status is rare. Consequently, doing so
using MOVCRW/MOVWCR or
PUSHCR/POPCR is expected to be adequate.
| Instruction | FPU Status Register (FSR) | ||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| FSR[28:24] | FSR[19:16] | FSR[14:8] | FSR[6:0] | ||||||||||||||||||||
| SUB | INF | FN | FZ | FNAN | GT | LT | EQ | UN | SUBOS | HUGIS | INXS | UDFS | OVFS | DIVOS | INVALS | ||||||||
| Move Instructions | |||||||||||||||||||||||
FMOV | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — |
FMOVC | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — |
| Status Bit Set/Clear/Update Instructions | |||||||||||||||||||||||
FAND
(1) | — | — | — | — | — | — | — | — | — | ⇓ | ⇓ | ⇓ | ⇓ | ⇓ | ⇓ | ⇓ | ⇓ | ⇓ | ⇓ | ⇓ | ⇓ | ⇓ | ⇓ |
FIOR
(1) | — | — | — | — | — | — | — | — | — | ⇑ | ⇑ | ⇑ | ⇑ | ⇑ | ⇑ | ⇑ | ⇑ | ⇑ | ⇑ | ⇑ | ⇑ | ⇑ | ⇑ |
FTST | ⇕ | ⇕ | ⇕ | ⇕ | ⇕ | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — | — |
| Conversion Instructions | |||||||||||||||||||||||
FLI2F | — | — | — | — | — | — | — | — | — | — | — | ⇑(2) | — | — | — | — | 0 | 0 | ⇕(2) | 0 | 0 | 0 | 0 |
FDI2F | — | — | — | — | — | — | — | — | — | — | — | ⇑ | — | — | — | — | 0 | 0 | ⇕ | 0 | 0 | 0 | 0 |
FF2LI | — | — | — | — | — | — | — | — | — | ⇑ | ⇑ | ⇑ | — | — | — | ⇑ | ⇕ | ⇕ | ⇕ | 0 | 0 | 0 | ⇕ |
FF2DI | — | — | — | — | — | — | — | — | — | ⇑ | ⇑ | ⇑ | — | — | — | ⇑ | ⇕ | ⇕ | ⇕ | 0 | 0 | 0 | ⇕ |
| Comparison Instructions | |||||||||||||||||||||||
FCPS | — | — | — | — | — | ⇕ | ⇕ | ⇕ | ⇕ | ⇑ | — | — | — | — | — | ⇑ | ⇕ | 0 | 0 | 0 | 0 | 0 | ⇕ |
FCPQ | — | — | — | — | — | ⇕ | ⇕ | ⇕ | ⇕ | ⇑ | — | — | — | — | — | ⇑ | ⇕ | 0 | 0 | 0 | 0 | 0 | ⇕ |
FFLIM | — | — | — | — | — | — | — | — | — | ⇑ | — | — | — | — | — | ⇑ | ⇕ | 0 | 0 | 0 | 0 | 0 | ⇕ |
FMAX | — | — | — | — | — | — | — | — | — | ⇑ | — | — | — | — | — | ⇑ | ⇕ | 0 | 0 | 0 | 0 | 0 | ⇕ |
FMAXNUM | — | — | — | — | — | — | — | — | — | ⇑ | — | — | — | — | — | ⇑ | ⇕ | 0 | 0 | 0 | 0 | 0 | ⇕ |
FMIN | — | — | — | — | — | — | — | — | — | ⇑ | — | — | — | — | — | ⇑ | ⇕ | 0 | 0 | 0 | 0 | 0 | ⇕ |
FMINNUM | — | — | — | — | — | — | — | — | — | ⇑ | — | — | — | — | — | ⇑ | ⇕ | 0 | 0 | 0 | 0 | 0 | ⇕ |
| Math Instructions | |||||||||||||||||||||||
FADD | — | — | — | — | — | — | — | — | — | ⇑ | — | ⇑ | ⇑ | ⇑ | — | ⇑ | ⇕ | 0 | ⇕ | ⇕ | ⇕ | 0 | ⇕ |
FSUB | — | — | — | — | — | — | — | — | — | ⇑ | — | ⇑ | ⇑ | ⇑ | — | ⇑ | ⇕ | 0 | ⇕ | ⇕ | ⇕ | 0 | ⇕ |
FNEG | — | — | — | — | — | — | — | — | — | ⇑ | — | — | — | — | — | — | ⇕ | — | — | — | — | — | — |
FABS | — | — | — | — | — | — | — | — | — | ⇑ | — | — | — | — | — | — | ⇕ | — | — | — | — | — | — |
FMUL | — | — | — | — | — | — | — | — | — | ⇑ | — | ⇑ | ⇑ | ⇑ | — | ⇑ | ⇕ | 0 | ⇕ | ⇕ | ⇕ | 0 | ⇕ |
FMAC | — | — | — | — | — | — | — | — | — | ⇑ | — | ⇑ | ⇑ | ⇑ | — | ⇑ | ⇕ | 0 | ⇕ | ⇕ | ⇕ | 0 | ⇕ |
FDIV | — | — | — | — | — | — | — | — | — | ⇑ | — | ⇑ | ⇑ | ⇑ | ⇑ | ⇑ | ⇕ | 0 | ⇕ | ⇕ | ⇕ | ⇕ | ⇕ |
FSQRT | — | — | — | — | — | — | — | — | — | ⇑ | — | ⇑ | — | — | — | ⇑ | ⇕ | 0 | ⇕ | 0 | 0 | 0 | ⇕ |
FSIN | — | — | — | — | — | — | — | — | — | ⇑ | — | ⇑ | ⇑ | — | — | ⇑ | ⇕ | 0 | ⇕ | ⇕ | 0 | 0 | ⇕ |
FCOS | — | — | — | — | — | — | — | — | — | ⇑ | — | ⇑ | ⇑ | — | — | ⇑ | ⇕ | 0 | ⇕ | ⇕ | 0 | 0 | ⇕ |
| Key: ⇕ set or cleared, ‘0’ always cleared, — unchanged, ⇓
may be cleared but never set, ⇑ may be set but never cleared Note:
| |||||||||||||||||||||||