FPU Execute Stage
Each instruction may consist of one or more execute stages depending upon the functional block targeted by the operation. When the instruction enters the X [0]-stage, it is registered such that the RD-stage is free to receive another instruction issued by the CPU.
All instructions (other than FDIV) are pipelined through as many X[n] stages as deemed necessary to meet the timing requirements.
The pipeline stages will be added such that the propagation delay of each is as balanced as possible, and the sequential issue of the same instruction may be fully pipelined (i.e., instructions using the same functional block may be sequentially issued without incurring a structural hazard in the Execute stage).