FPU WAR Hazards
The WAR (Write-After-Read) anti-dependency hazard can occur should the pipeline allow read and write execution to be out of (instruction sequence) order. That is, a WAR hazard will arise whenever an instruction writes to a register before the same register is read by a prior instruction. That is, the read and write occur out of execution order resulting in the (older) read instruction ultimately using the (later) write data which would be incorrect.
Under normal sequential execution conditions, a WAR hazard should never arise because the read of
all older instructions always precedes the writes of later ones. However, a WAR hazard
can arise within the coprocessor pipeline when a slow instruction (e.g., FPU
FSIN) has a result data dependency (RAW hazard) with a later instruction,
and that later instruction is followed by a MOVWCR or
POPCR instruction that targets the same register as the dependency.
This is because the dependency will force an FPU pipeline stall until the result data
are available and the RAW hazard is resolved, but the MOVWCR or
POPCR move instructions (which do not execute using the FPU
pipeline) will not be stalled. Consequently, it is possible that the write from the
MOVWCR or POPCR instruction would occur prior to
the stalled instruction continuing execution (after the RAW hazard). The write would
then be overwritten by the FPU pipeline and, therefore, lost. This scenario is detected
as a WAR hazard and prevented from happening by stalling the most recent write, such
that the write order remains correct. CPU to FPU move instructions that do not target
the register involved in the stall will still execute as normal (i.e., without
stalling).
The coprocessor must, therefore, detect the possibility of such a hazard and force in-order execution of all dependent instructions by stalling the most recent CPU write instruction in the W-stage until after the prior read is completed.
An example WAR hazard and its resolution are as follows: A RAW hazard between the
FSIN.s and FMOV.s instructions will stall
FMOV.s to resolve the hazard (stall cycles shown in green), but
this will also set the pipeline up for a possible WAR hazard because the subsequent
MOVWCR instruction is not prevented from continuing execution.
As is the case in this example, should the MOVWCR instruction destination be the
same F-reg as that used by the FMOV.s as a source, the
MOVWCR must be prevented from writing until the prior
(FSIN.s) has been able to forward the write data to the
MOV.s RD-stage. The FSIN.s and
MOVWCR enter their respective write stages together, and the FPU
prioritizes the CPU write, maintaining correct write ordering. This results in a
one-cycle stall of the MOVWCR instruction to resolve the hazard.