3.1.11.2 WPS Mode Demo Console Log
Note: In the WPS button method, the
following information will be displayed on the terminal window.
-- WINC1500 security connection with Wi-Fi Protected Setup(WPS) example -- -- XXXXX_XPLAINED_PRO -- -- Compiled: xxx x xxxx xx:xx:xx -- (APP)(INFO)Chip ID 1503a0 (APP)(INFO)Firmware ver : xx.x.x Svnrev xxxxx (APP)(INFO)Firmware Build xxx x xxxx Time xx:xx:xx (APP)(INFO)Firmware Min driver ver : xx.x.x (APP)(INFO)Driver ver: xx.x.x (APP)(INFO)Driver built at xxx x xxxx xx:xx:xx SW0 button pressed Device is connecting using WPS Push Button option Wi-Fi request WPS SSID : xxxxxx, AuthType : x, PW : xxxxxxxx Request Wi-Fi connect Wi-Fi connected Wi-Fi IP is xxx.xxx.xxx.xxx
Note: In the WPS PIN method, the
following information will be displayed on the terminal window.
-- WINC1500 security connection with Wi-Fi Protected Setup(WPS) example -- -- XXXXX_XPLAINED_PRO -- -- Compiled: xxx x xxxx xx:xx:xx -- (APP)(INFO)Chip ID 1503a0 (APP)(INFO)Firmware ver : xx.x.x Svnrev xxxxx (APP)(INFO)Firmware Build xxx x xxxx Time xx:xx:xx (APP)(INFO)Firmware Min driver ver : xx.x.x (APP)(INFO)Driver ver: xx.x.x (APP)(INFO)Driver built at xxx x xxxx xx:xx:xx Wi-Fi request WPS SSID : xxxxxx, AuthType : x, PW : xxxxxxxx Request Wi-Fi connect Wi-Fi connected Wi-Fi IP is xxx.xxx.xxx.xxx