3.1.2.2 Get MAC Address Demo Console Log
The application should now be programmed and running. The following information will be displayed on the terminal window.
-- WINC1500 MAC Address example -- -- XXXXX_XPLAINED_PRO -- -- Compiled: xxx x xxxx xx:xx:xx -- (APP)(INFO)Chip ID 1503a0 (APP)(INFO)Firmware ver : xx.x.x Svnrev xxxxx (APP)(INFO)Firmware Build xxx x xxxx Time xx:xx:xx (APP)(INFO)Firmware Min driver ver : xx.x.x (APP)(INFO)Driver ver: xx.x.x (APP)(INFO)Driver built at xxx x xxxx xx:xx:xx OTP MAC Address : F8:F0:05:F2:5F:62
Note:
- The default MAC address is stored in One-Time-Programmable ROM (OTP ROM).
- The output of this example should display the OTP MAC address or USER MAC address.
- User defined MAC address: If you want to use a custom MAC address, there is an API available which allows for setting a user defined MAC address.