Once your sensor Wi-Fi module is provisioned, connect your Android device to
the same Access Point and open the Atmel IoT Sensor Application. Your sensor will
display on the Android application’s main screen as shown below:Figure 5-10. Demo Android App
By tapping the sensor’s name, you will be able to access the real time data
flow. In the case of a temperature sensor, you can see the real time temperature data in
the graph. The “LED Toggle” button toggles the LED status. A green or red light next to
the “LED Toggle” button gives the current status of the LED.
Note: If your Android device is not
connected to the same Access Point as the sensor, you will not be able see any
device.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.