1.2.3.4.2 SYS_CMD_ADDGRP Function
C
bool SYS_CMD_ADDGRP(const SYS_CMD_DESCRIPTOR* pCmdTbl, int nCmds,
const char* groupName,
const char* menuStr)Summary
Allows clients to add command process to the Command Processor System Service.
Description
Client modules may call this function to add command process to the Command Processor System Service.
Precondition
SYS_CMD_Initialize was successfully run once.
Parameters
None.
Example
static const SYS_CMD_DESCRIPTOR cmdTbl= { {"command_as_typed_at_the_prompt", _Function_Name_That_Supports_The_Command, ": Helpful description of the command for the user"}, };
bool APP_AddCommandFunction() { if (!SYS_CMD_ADDGRP(cmdTbl, sizeof(cmdTbl)/sizeof(*cmdTbl), "Command Group Name", ": Command Group Description")) { return false; } return true; }
Returns
true - Indicates success
false - Indicates an error occurred
Remarks
None.