1.2.3.4.1 SYS_CMD_Initialize Function
C
bool SYS_CMD_Initialize( const SYS_MODULE_INIT * const init )Summary
Initializes data for the instance of the Command Processor module.
Description
This function initializes the Command Processor module. It also initializes any internal data structures.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| init | Pointer to a data structure containing any data necessary to initialize the sys command. This pointer may be null if no data is required because static overrides have been provided. |
Returns
true - Indicates success
false - Indicates an error occurred
Remarks
This routine should only be called once during system initialization.