1.3.3.1.6 MAC_COMMON_GetRequestSync Function
C
MAC_STATUS MAC_COMMON_GetRequestSync
(
MAC_COMMON_PIB_ATTRIBUTE attribute,
uint16_t index,
MAC_PIB_VALUE *pibValue
);
Summary
The MAC_COMMON_GetRequestSync primitive gets the value of an attribute in the MAC Common layer Parameter Information Base (PIB).
Description
GetRequestSync primitive is used to get the value of a PIB. Sync suffix indicates that result is provided upon function call return, in the pibValue parameter.
Precondition
MAC_COMMON_Init primitive has to be called before.
Parameters
| Param | Description |
|---|---|
| attribute | Identifier of the Attribute to retrieve value. |
| index | Index of element in case Attribute is a table. Otherwise index must be set to '0'. |
| pibValue | Pointer to MAC_PIB_VALUE object where value will be returned. |
Returns
Result of get operation as a MAC_STATUS code.
Example
MAC_STATUS status;
MAC_PIB_VALUE value;
status = MAC_COMMON_GetRequestSync(MAC_COMMON_PIB_RC_COORD, 0, &value);
if (status == MAC_STATUS_SUCCESS)
{
// Get value from 'value' parameter
}
Remarks
None.