1.3.3.1.15 MAC_StartConfirm Typedef
C
typedef void (*MAC_StartConfirm)(MAC_START_CONFIRM_PARAMS *scParams);
Summary
Pointer to a Start Confirm Event handler function.
Description
This data type defines the required function signature for the MAC Start Confirm event handling callback function. A client must register a pointer using the event handling function whose function signature (parameter and return value types) matches the types specified by this function pointer in order to receive Start Confirm events back from module.
Parameters
| Param | Description |
|---|---|
| scParams | Pointer to structure containing parameters related to Confirm. See MAC_START_CONFIRM_PARAMS. |
Returns
None.
Example
App_StartConfirm(MAC_START_CONFIRM_PARAMS *params)
{
// Check result
if (params->status != MAC_STATUS_SUCCESS)
{
// Handle Start error
}
else
{
// Start performed correctly. PAN Coordinator ready.
}
}
Remarks
None.