1.3.3.1.23 MAC_COMMON_GetMsCounter Function
C
uint32_t MAC_COMMON_GetMsCounter
(
void
);
Summary
The MAC_COMMON_GetMsCounter primitive gets the value of a counter that is incremented every millisecond.
Description
This primitive makes use of SYS_TIME service to get the value of the millisecond counter in order to be able to set timeouts and perform delays. This function returns the current value of such counter.
Precondition
SYS_TIME_Initialize primitive has to be called before.
Parameters
None.
Returns
Value of milliseconds counter.
Example
previousCounter = MAC_COMMON_GetMsCounter();
// Perform other actions
// ...
newCounter = MAC_COMMON_GetMsCounter();
if ((newCounter - previousCounter) > TIMEOUT_MS)
{
// Timeout elapsed
}
Remarks
None.