1.3.3.1.13 MAC_ScanConfirm Typedef
C
typedef void (*MAC_ScanConfirm)(MAC_SCAN_CONFIRM_PARAMS *scParams);
Summary
Pointer to a Scan Confirm Event handler function.
Description
This data type defines the required function signature for the MAC Scan Confirm event handling callback function. A client must register a pointer using the event handling function whose function signature (parameter and return value types) matches the types specified by this function pointer in order to receive Scan Confirm events back from module.
Parameters
| Param | Description |
|---|---|
| scParams | Pointer to structure containing parameters related to Confirm. See MAC_SCAN_CONFIRM_PARAMS. |
Returns
None.
Example
App_ScanConfirm(MAC_SCAN_CONFIRM_PARAMS *params)
{
// Check result
if (params->status != MAC_STATUS_SUCCESS)
{
// Handle Scan error
}
else
{
// Scan performed correctly
// Check received Beacons
}
}
Remarks
None.