1.3.3.1.7 MAC_COMMON_SetRequestSync Function
C
MAC_STATUS MAC_COMMON_SetRequestSync
(
MAC_COMMON_PIB_ATTRIBUTE attribute,
uint16_t index,
const MAC_PIB_VALUE *pibValue
);
Summary
The MAC_COMMON_SetRequestSync primitive sets the value of an attribute in the MAC Common layer Parameter Information Base (PIB).
Description
SetRequestSync primitive is used to set the value of a PIB. Sync suffix indicates that result of set operation is provided upon function call return, in the return status code.
Precondition
MAC_COMMON_Init primitive has to be called before.
Parameters
| Param | Description |
|---|---|
| attribute | Identifier of the Attribute to provide value. |
| index | Index of element in case Attribute is a table. Otherwise index must be set to '0'. |
| pibValue | Pointer to MAC_PIB_VALUE object where value is contained. |
Returns
Result of set operation as a MAC_STATUS code.
Example
MAC_STATUS status;
const MAC_PIB_VALUE value = {
.length = 2,
.value = {0xFF, 0xFF}
};
status = MAC_COMMON_SetRequestSync(MAC_COMMON_PIB_RC_COORD, 0, &value);
if (status == MAC_STATUS_SUCCESS)
{
// PIB correctly set
}
Remarks
None.