1.3.3.1.45 MAC_TONE_MAP Struct

C

typedef struct
{
    uint8_t toneMap[(MAX_TONE_GROUPS + 7) / 8];
} MAC_TONE_MAP;

Summary

Defines the G3 Tone Map at Mac level.

Description

Tone Map is a bitmap in which each bit represents one of the subbands present in the PLC work band (6 subbands in CEN-A, 4 subbands in CEN-B, 24 subbands in FCC). '1' indicates the subband is used, '0' indicates the subband is not used.

Field description:

  • toneMap: Array of bytes containing the bitmap explained above

Remarks

It is only used when PLC MAC layer is present.