15.2 Warnings
The list of warnings is as follows:
- An appropriate disconnect device shall be incorporated in the building installation wiring
- Do not use a cross-over cable between the PD-IES-xyy output port and the load device.
- Take extra care when connecting the AC power, so that N, L, and Ground, are connected to the proper polarity.
- Ensure that the input voltage is within the allowed range.
- Verify that all high input voltage terminals are properly insulated and not exposed.