2.6.1 Native Interface Transactions
(Ask a Question)This section describes the read/write rules and sequences in the native interface. For information about native interface signals, see Table 2-10.
Important: During the simulation,
users can find the difference between Core configuration timings (JEDEC®) and
simulation results. This is due to the internal architecture of the controller (T4), which
includes a 4-stage queue so that commands to memory are issued at every 4 clock
cycles.