The Timer/Counter is a synchronous design
and the timer clock (clkT1) is
therefore shown as a clock enable signal in the following figures. The figures include
information on when Interrupt Flags are set, and when the OCR1x Register is updated with the OCR1x buffer value (only
for modes utilizing double buffering). The first figure shows a timing diagram for the
setting of OCF1x.
Figure 1. Timer/Counter Timing Diagram,
Setting of OCF1x, no Prescaling
Note: The “n” in the register and bit names indicates the device number (n = 1 for Timer/Counter 1), and the “x” indicates Output Compare unit (A/B).
The next figure shows the same timing data,
but with the prescaler enabled.
Figure 2. Timer/Counter Timing Diagram,
Setting of OCF1x, with Prescaler (fclk_I/O/8)
Note: The “n” in the register and bit names indicates the device number (n = 1 for Timer/Counter 1), and the “x” indicates Output Compare unit
(A/B).
The next figure shows the count sequence
close to TOP in various modes. When using phase and frequency correct PWM mode the OCR1x Register is updated at BOTTOM. The timing diagrams will be
the same, but TOP should be replaced by BOTTOM, TOP-1 by BOTTOM+1 and so on. The same
renaming applies for modes that set the TOV1 Flag at
BOTTOM.
Figure 3. Timer/Counter Timing Diagram, no
Prescaling.
Note: The “n” in the register and bit names indicates the device number (n = 1 for Timer/Counter 1), and the “x” indicates Output Compare unit
(A/B).
The next figure shows the same timing data,
but with the prescaler enabled.
Figure 4. Timer/Counter Timing Diagram, with
Prescaler (fclk_I/O/8)
Note: The “n” in the register and bit names indicates the device number (n = 1 for Timer/Counter 1), and the “x” indicates Output Compare unit
(A/B).