27.6.4 Interrupt Enable Clear

Name: INTENCLR
Offset: 0x0C
Reset: 0x0000
Property: PAC Write-Protection

Bit 15141312111098 
      SEEWRCSEESOVFSEESFULL 
Access R/WR/WR/W 
Reset 000 
Bit 76543210 
 SUSPNVMEECCDEECCSELOCKEPROGEADDREDONE 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000000 

Bit 10 – SEEWRC SEE Write Completed Interrupt Clear

Writing a zero to this bit has no effect.

Writing a '1' to this bit clears the SEEWRC interrupt enable.

This bit will read as the current value of the SEEWRC interrupt enable.

Bit 9 – SEESOVF Active SEES Overflow Interrupt Clear

Writing a zero to this bit has no effect.

Writing a '1' to this bit clears the SEESOVF interrupt enable.

This bit will read as the current value of the SEESOVF interrupt enable.

Bit 8 – SEESFULL Active SEES Full Interrupt Clear

Writing a zero to this bit has no effect.

Writing a '1' to this bit clears the SEESFULL interrupt enable.

This bit will read as the current value of the SEESFULL interrupt enable.

Bit 7 – SUSP Suspended Write Or Erase Interrupt Clear

Writing a zero to this bit has no effect.

Writing a '1' to this bit clears the SUSP interrupt enable.

This bit will read as the current value of the SUSP interrupt enable.

Bit 6 – NVME NVM Error Interrupt Clear

Writing a zero to this bit has no effect.

Writing a '1' to this bit clears the NVME interrupt enable.

This bit will read as the current value of the NVME interrupt enable.

Bit 5 – ECCDE ECC Dual Error Interrupt Clear

Writing a zero to this bit has no effect.

Writing a '1' to this bit clears the ECCDE interrupt enable.

This bit will read as the current value of the ECCDE interrupt enable.

Bit 4 – ECCSE ECC Single Error Interrupt Clear

Writing a zero to this bit has no effect.

Writing a '1' to this bit clears the ECCSE interrupt enable.

This bit will read as the current value of the ECCSE interrupt enable.

Bit 3 – LOCKE Lock Error Interrupt Clear

Writing a zero to this bit has no effect.

Writing a '1' to this bit clears the LOCKE interrupt enable.

This bit will read as the current value of the LOCKE interrupt enable.

Bit 2 – PROGE Programming Error Interrupt Clear

Writing a zero to this bit has no effect.

Writing a '1' to this bit clears the PROGE interrupt enable.

This bit will read as the current value of the PROGE interrupt enable.

Bit 1 – ADDRE Address Error Interrupt Clear

Writing a zero to this bit has no effect.

Writing a '1' to this bit clears the ADDRE interrupt enable.

This bit will read as the current value of the ADDRE interrupt enable.

Bit 0 – DONE Command Done Interrupt Clear

Writing a zero to this bit has no effect.

Writing a '1' to this bit clears the DONE interrupt enable.

This bit will read as the current value of the DONE interrupt enable.