27.6.6 Interrupt Flag Status and Clear

Name: INTFLAG
Offset: 0x10
Reset: 0x0000
Property: -

Bit 15141312111098 
      SEEWRCSEESOVFSEESFULL 
Access R/WR/WR/W 
Reset 000 
Bit 76543210 
 SUSPNVMEECCDEECCSELOCKEPROGEADDREDONE 
Access R/WR/WRRR/WR/WR/WR/W 
Reset 00000000 

Bit 10 – SEEWRC SEE Write Completed

0: AHB write is pending.

1: AHB write has completed, and NVM is programmed with correct values.

Bit 9 – SEESOVF Active SEES Overflow

0: No SEES overflow have been detected since the last clear.

1: At least SEES overflow has been detected since the last clear.

This bit can be cleared by writing a one to its bit location.

Bit 8 – SEESFULL Active SEES Full

0: The active SEES is not full

1: The active SEES is Full, meaning that the next write will fail if the active sector is not reallocated.

This bit can be cleared by writing a one to its bit location.

Bit 7 – SUSP Suspended Write Or Erase Operation

0: No write/suspend has occurred since the last clear.

1: A write or erase operation has been suspended since the last clear.

This bit can be cleared by writing a one to its bit location.

Bit 6 – NVME NVM Error

0: No NVM errors have been received since the last clear.

1: At least one NVM error has occurred since the last clear.

This bit can be cleared by writing a one to its bit location.

Bit 5 – ECCDE ECC Dual Error

0: No ECC dual errors have been received since the last ECCERR register read.

1: At least one ECC error has occurred since the last ECCERR register read.

This bit is cleared when the ECCERR register is read.

Bit 4 – ECCSE ECC Single Error

0: No ECC single errors have been received since the last ECCERR register read.

1: At least one ECC error has occurred since the last ECCERR register read.

This bit is cleared when the ECCERR register is read.

Bit 3 – LOCKE Lock Error

0: No LOCK errors have been received since the last clear.

1: At least one LOCK error has occurred since the last clear.

This bit can be cleared by writing a one to its bit location.

Bit 2 – PROGE Programming Error

0: No PROG errors have been received since the last clear.

1: At least one PROG error has occurred since the last clear.

This bit can be cleared by writing a one to its bit location.

Bit 1 – ADDRE Address Error

0: No ADDRE error has been detected since the last clear.

1: At least one ADDRE error has been detected since the last clear.

This bit can be cleared by writing a one to its bit location.

Bit 0 – DONE Command Done

0: The NVM controller has not completed any command since the last clear.

1: At least one command has completed since the last clear.

This bit can be cleared by writing a one to its bit location.