6.18.46 tmpfile Function
Creates a temporary file.
Attention: This function is not
implemented by MPLAB XC8.
Include
<stdio.h>
Prototype
FILE * tmpfile(void)
Return Value
Returns a stream pointer if successful; otherwise, returns a NULL
pointer.
Remarks
tmpfile creates a file with a unique filename. The temporary file is
opened in w+b (binary read/write) mode. It will automatically be
removed when exit is called; otherwise the file will remain in the directory. This
function requires a heap.
Example
#include <stdio.h>
int main(void)
{
FILE *mytempfile;
if ((mytempfile = tmpfile()) == NULL)
printf("Cannot create temporary file");
else
printf("Temporary file was created");
}
Example Output
Temporary file was created