6.18.28 fwrite Function
Writes data to the stream.
Include
<stdio.h>
Prototype
size_t fwrite(const void * restrict ptr, size_t size, size_t
nelem, FILE * restrict stream);
Arguments
ptr- pointer to the storage buffer
size- size of item
nelem- maximum number of items to be read
stream- pointer to the open stream
Return Value
Returns the number of complete elements successfully
written, which will be less than nelem only if a write
error is encountered.
Remarks
The function writes characters to a given stream from a
buffer pointed to by ptr up to nelem
elements whose size is specified by size. The file position indicator is
advanced by the number of characters successfully written. If the function
sets the error indicator, the file-position indicator is
indeterminate.
Example
#include <stdio.h>
int main(void)
{
FILE *buf;
int x, numwrote, numread;
double nums[10], readnums[10];
if ((buf = fopen("afile.out", "w+")) != NULL)
{
for (x = 0; x < 10; x++)
{
nums[x] = 10.0/(x + 1);
printf("10.0/%d = %f\n", x+1, nums[x]);
}
numwrote = fwrite(nums, sizeof(double), 10, buf);
printf("Wrote %d numbers\n\n", numwrote);
fclose(buf);
}
else
printf("Cannot open afile.out\n");
if ((buf = fopen("afile.out", "r+")) != NULL)
{
numread = fread(readnums, sizeof(double), 10, buf);
printf("Read %d numbers\n", numread);
for (x = 0; x < 10; x++)
{
printf("%d * %f = %f\n", x+1, readnums[x],
(x + 1) * readnums[x]);
}
fclose(buf);
}
else
printf("Cannot open afile.out\n");
}
Example Output
10.0/1 = 10.000000
10.0/2 = 5.000000
10.0/3 = 3.333333
10.0/4 = 2.500000
10.0/5 = 2.000000
10.0/6 = 1.666667
10.0/7 = 1.428571
10.0/8 = 1.250000
10.0/9 = 1.111111
10.0/10 = 1.000000
Wrote 10 numbers
Read 10 numbers
1 * 10.000000 = 10.000000
2 * 5.000000 = 10.000000
3 * 3.333333 = 10.000000
4 * 2.500000 = 10.000000
5 * 2.000000 = 10.000000
6 * 1.666667 = 10.000000
7 * 1.428571 = 10.000000
8 * 1.250000 = 10.000000
9 * 1.111111 = 10.000000
10 * 1.000000 = 10.000000
Example Explanation
This program uses fwrite to save 10 numbers
to a file in binary form. This allows the numbers to be saved in the same
pattern of bits as the program is using which provides more accuracy and
consistency. Using fprintf would save the numbers as text
strings, which could cause the numbers to be truncated. Each number is
divided into 10 to produce a variety of numbers. Retrieving the numbers
with fread to a new array and multiplying them by the
original number shows the numbers were not truncated in the save
process.