6.18.12 feof Function
Tests for end-of-file.
Include
<stdio.h>
Prototype
int feof(FILE * stream);
Argument
stream- stream to check for end-of-file
Return Value
Returns non-zero if stream end-of-file indicator is set; otherwise, returns zero.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
int main(void)
{
FILE * myfile;
int y = 0;
if( (myfile = fopen( "afile.txt", "rb" )) == NULL )
printf( "Cannot open file\n" );
else
{
for (;;)
{
y = fgetc(myfile);
if (feof(myfile))
break;
fputc(y, stdout);
}
fclose( myfile );
}
}
Example Input
Contents of afile.txt (used as input):
This is a sentence.
Example Output
This is a sentence.