6.18.35 putchar Function
Put a character to stdout.
Include
<stdio.h>
Prototype
int putchar(int c);
Argument
c- character to be written
Return Value
Returns the character or EOF if an error occurs or end-of-file is
reached.
Remarks
Same effect as fputc with stdout as an argument.
When building with the MPLAB XC8 compiler for PIC MCUs, the putchar()
function relies on the putch() function being properly defined to
direct output to the required peripheral or location. Printing will not work as expected
until the putch() stub (found in the
pic/sources/c99/common/putch.c of your compiler distribution)
is completed. See Example code for 8-bit PIC MCUs
for information on defining putch() so that printed text appears in an
MPLAB X IDE simulator window.
Example
#include <stdio.h>
int main(void)
{
char *y;
char buf[] = "This is text\n";
int x;
x = 0;
for (y = buf; (x != EOF) && (*y != '\0'); y++)
x = putchar(*y);
}
Example Output
This is text