6.18.34 putc Function
Puts a character to the stream.
Attention: This function is not implemented
by MPLAB XC8 for PIC MCUs. It is implemented by all other compilers, but MPLAB XC8 for
AVR MCUs has limited support of data streams.
Include
<stdio.h>
Prototype
int putc(int c, FILE * stream);
Arguments
c- character to be written
stream- pointer to
FILEstructure
Return Value
Returns the character or EOF if an error occurs or end-of-file is
reached.
Remarks
The putc function performs the same task as the function
fputc.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
int main(void)
{
char *y;
char buf[] = "This is text\n";
int x;
x = 0;
for (y = buf; (x != EOF) && (*y != '\0'); y++)
{
x = putc(*y, stdout);
putc('|', stdout);
}
}
Example Output
T|h|i|s| |i|s| |t|e|x|t|
|