6.18.14 fflush Function
Flushes the buffer in the specified stream.
Attention: This function is not implemented
by MPLAB XC8 for PIC MCUs. It is implemented by all other compilers, but MPLAB XC8 for
AVR MCUs has limited support of data streams.
Include
<stdio.h>
Prototype
int fflush(FILE * stream);
Argument
stream- pointer to the stream to flush
Return Value
Returns EOF if a write error occurs; otherwise, returns zero for
success.
Remarks
If stream is a null pointer, all output buffers are written to files. The
fflush function has no effect on an unbuffered stream.