6.18.16 fgetpos Function
Gets the stream’s file position.
Include
<stdio.h>
Prototype
int fgetpos(FILE * stream, fpos_t * pos);
Arguments
stream- target stream
pos- position-indicator storage
Return Value
Returns 0 if successful; otherwise, returns a non-zero value.
Remarks
The function stores the file-position indicator for the given stream into the object pointed
to by pos if successful; otherwise, fgetpos sets
errno.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
/* This program opens a file and reads bytes at */
/* several different locations. The fgetpos */
/* function notes the 8th byte. 21 bytes are */
/* read then 18 bytes are read. Next the */
/* fsetpos function is set based on the */
/* fgetpos position and the previous 21 bytes */
/* are reread. */
#include <stdio.h>
int main(void)
{
FILE *myfile;
fpos_t pos;
char buf[25];
if ((myfile = fopen("sampfgetpos.c", "rb")) == NULL)
printf("Cannot open file\n");
else
{
fread(buf, sizeof(char), 8, myfile);
if (fgetpos(myfile, &pos) != 0)
perror("fgetpos error");
else
{
fread(buf, sizeof(char), 21, myfile);
printf("Bytes read: %.21s\n", buf);
fread(buf, sizeof(char), 18, myfile);
printf("Bytes read: %.18s\n", buf);
}
if (fsetpos(myfile, &pos) != 0)
perror("fsetpos error");
fread(buf, sizeof(char), 21, myfile);
printf("Bytes read: %.21s\n", buf);
fclose(myfile);
}
}
Example Output
Bytes read: program opens a file
Bytes read: and reads bytes at
Bytes read: program opens a file