6.18.17 fgets Function
Get a string from a stream.
Include
<stdio.h>
Prototype
char * fgets(char * s, int n, FILE * stream);
Arguments
s- pointer to the storage string
n- maximum number of characters to read
stream- pointer to the open stream
Return Value
Returns a pointer to the string s if successful; otherwise, returns a null
pointer.
Remarks
The function reads characters from the input stream and stores them into the
string pointed to by s until it has read n-1 characters,
stores a newline character or sets the end-of-file or error indicators. If any characters were
stored, a null character is stored immediately after the last read character in the next
element of the array. If fgets sets the error indicator, the array contents
are indeterminate.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
#define MAX 50
int main(void)
{
FILE *buf;
char s[MAX];
if ((buf = fopen("afile.txt", "r")) == NULL)
printf("Cannot open afile.txt\n");
else
{
while (fgets(s, MAX, buf) != NULL)
printf("%s|", s);
fclose(buf);
}
}
Example Input
Contents of afile.txt (used as input):
Short
Longer string
Example Output
Short
|Longer string
|