6.18.27 ftell Function
Gets the current position of a file pointer.
Attention: This function is not
implemented by MPLAB XC8.
Include
<stdio.h>
Prototype
long ftell(FILE * stream);
Argument
stream- stream in which to get the current file position
Return Value
Returns the position of the file pointer if successful; otherwise, returns -1.
Example
#include <stdio.h>
int main(void)
{
FILE *myfile;
char s[75];
long y;
myfile = fopen("afile.out", "w+");
if (myfile == NULL)
printf("Cannot open afile.out\n");
else
{
fprintf(myfile,"This is a very long sentence "
"for input into the file named afile.out for testing.");
fclose(myfile);
if ((myfile = fopen("afile.out", "rb")) != NULL)
{
printf("Read some characters:\n");
fread(s, sizeof(char), 29, myfile);
printf("\t\"%s\"\n", s);
y = ftell(myfile);
printf("The current position of the file pointer is %ld\n", y);
fclose(myfile);
}
}
}
Example Output
Read some characters:
"This is a very long sentence "
The current position of the file pointer is 29