6.18.5 stdio Macros
BUFSIZ
An integer constant expression that is the size of the buffer used by the
setbuf() function
Include
#include <stdio.h>
EOF
An integer constant expression, with type int and a negative value,
that is returned by several file-access functions to indicate end-of-file, that is,
no more input from a stream.
Include
#include <stdio.h>
FILENAME_MAX
An integer constant expression that when used as the size of a char
array will ensure that that array can hold the longest file name string that can be
opened.
Include
#include <stdio.h>
FOPEN_MAX
An integer constant expression that is the minimum number of files that can be open simultaneously.
Include
#include <stdio.h>