6.18.21 fputs Function
Puts a string to the stream.
Attention: This function is not implemented
by MPLAB XC8 for PIC MCUs. It is implemented by all other compilers, but MPLAB XC8 for
AVR MCUs has limited support of data streams.
Include
<stdio.h>
Prototype
int fputs(const char * restrict s, FILE * restrict stream);
Arguments
s- string to be written
stream- pointer to the open stream
Return Value
Returns a non-negative value if successful; otherwise, returns EOF.
Remarks
The function writes characters to the output stream up to but not including the null character.
Example
#include <stdio.h>
int main(void)
{
char buf[] = "This is text\n";
fputs(buf,stdout);
fputs("|",stdout);
}
Example Output
This is text
|