6.18.22 fread Function
Reads data from the stream.
Include
<stdio.h>
Prototype
size_t fread(void * restrict ptr, size_t size, size_t nelem, FILE
* restrict stream);
Arguments
ptr- pointer to the storage buffer
size- size of item
nelem- maximum number of items to be read
stream- pointer to the stream
Return Value
Returns the number of complete elements read up to nelem whose
size is specified by size.
Remarks
The function reads characters from a given stream into the buffer pointed to by
ptr until the function stores size * nelem characters or
sets the end-of-file or error indicator. fread returns n/size where n is the
number of characters it read. If n is not a multiple of size, the value of the last element is
indeterminate. If the function sets the error indicator, the file-position indicator is
indeterminate.
Example
#include <stdio.h>
int main(void) {
FILE *buf;
int x, numwrote, numread;
double nums[10], readnums[10];
if ((buf = fopen("afile.out", "w+")) != NULL) {
for (x = 0; x < 10; x++) {
nums[x] = 10.0/(x + 1);
printf("10.0/%d = %f\n", x+1, nums[x]);
}
numwrote = fwrite(nums, sizeof(double), 10, buf);
printf("Wrote %d numbers\n\n", numwrote);
fclose(buf);
}
else printf("Cannot open afile.out\n");
if ((buf = fopen("afile.out", "r+")) != NULL) {
numread = fread(readnums, sizeof(double), 10, buf);
printf("Read %d numbers\n", numread);
for (x = 0; x < 10; x++) {
printf("%d * %f = %f\n", x+1, readnums[x], (x + 1) * readnums[x]);
}
fclose(buf);
}
else printf("Cannot open afile.out\n");
}
Example Output
10.0/1 = 10.000000
10.0/2 = 5.000000
10.0/3 = 3.333333
10.0/4 = 2.500000
10.0/5 = 2.000000
10.0/6 = 1.666667
10.0/7 = 1.428571
10.0/8 = 1.250000
10.0/9 = 1.111111
10.0/10 = 1.000000
Wrote 10 numbers
Read 10 numbers
1 * 10.000000 = 10.000000
2 * 5.000000 = 10.000000
3 * 3.333333 = 10.000000
4 * 2.500000 = 10.000000
5 * 2.000000 = 10.000000
6 * 1.666667 = 10.000000
7 * 1.428571 = 10.000000
8 * 1.250000 = 10.000000
9 * 1.111111 = 10.000000
10 * 1.000000 = 10.000000
Example Explanation
This program uses fwrite to save 10 numbers to a file in
binary form. This allows the numbers to be saved in the same pattern of bits as the
program is using, which provides more accuracy and consistency. Using
fprintf would save the numbers as text strings, which could cause
the numbers to be truncated. Each number is divided into 10 to produce a variety of
numbers. Retrieving the numbers with fread to a new array and
multiplying them by the original number shows the numbers were not truncated in the save
process.