3.20.1 Recovery Method
If the PKOB4 becomes unresponsive, follow these steps to recover the tool:
- With the PIC32CM SG00/GC00 Curiosity
Pro development board still powered, short the 2 pads (marked in the following
figure) for approximately 10 seconds.
Figure 3-26. PKOB4 EBR Reset - Open the latest version of MPLAB X IDE.
- Click on the Projects tab and then select the project.
- From the main menu, click Debug, the Debug Project properties page will be displayed.
- Select Hardware Tool Emergency
Boot Firmware Recovery.
Figure 3-27. MPLAB X IDE Interface - Follow the onscreen instructions to reset the tool to factory conditions.
For additional information on PKOB4, refer to the “MPLAB® PICkit4 User’s Guide" (DS50002751), which is available for download at the following location.