5.4.4 Branching
The branching instructions add an offset to the PC. This allows relocatable code and
code that crosses page boundaries. There are two forms of branching,
BRW and BRA. The PC will have incremented to fetch
the next instruction in both cases. When using either branching instruction, a PCL
memory boundary may be crossed.
If using BRW, load the W register with the desired unsigned
address and execute BRW. The entire PC will be loaded with the address
PC + 1 + W.
If using BRA, the entire PC will be loaded with PC + 1 +
the signed value of the operand of the BRA instruction.