7.3.2 Running IAP Program

To run IAP with programming images, perform the following steps:

  1. Press 5 to initiate Program Device with IAP image1. The IAP program with image1 is executed successfully and the design version 02 with different silicon signature is displayed as shown in the following figure. This operation takes few seconds.
    Figure 7-17. Successful IAP with Image1
  2. Press 6 to initiate Program Device with IAP image2. The IAP program with image2 is executed successfully and the design version 03 with different silicon signature is displayed as shown in the following figure. This operation takes a few seconds.
    Figure 7-18. Successful IAP by Image2

This concludes running the IAP Program with images.