7.3.1 Running IAP Authentication

To run the IAP authentication, perform the following steps:

  1. Press 3 to initiate the IAP image1 authentication. The IAP authentication with image at index 2 is executed successfully. Tera Term displays the status code as shown in the following figure.
    Figure 7-15. Successful IAP Image1 Authentication
  2. Press 4 to initiate the IAP image2 authentication. The IAP authentication with image at index 3 is executed successfully. Tera Term displays the status code, as shown in the following figure.
    Figure 7-16. Successful IAP Image2 Authentication

This concludes the IAP image authentication.