10.6.3.2.3 Function nvm_read_buffer()
Reads a number of bytes from a page in the NVM memory region.
enum status_code nvm_read_buffer( const uint32_t source_address, uint8_t *const buffer, uint16_t length)
Reads a given number of bytes from a given page address in the NVM memory space into a buffer.
| Data direction | Parameter name | Description |
|---|---|---|
|
[in] |
source_address |
Source page address to read from |
|
[out] |
buffer |
Pointer to a buffer where the content of the read page will be stored |
|
[in] |
length |
Number of bytes in the page to read |
Returns
Status of the page read attempt.
| Return value | Description |
|---|---|
|
STATUS_OK |
Requested NVM memory page was successfully read |
|
STATUS_BUSY |
NVM controller was busy when the operation was attempted |
|
STATUS_ERR_BAD_ADDRESS |
The requested address was outside the acceptable range of the NVM memory region or not aligned to the start of a page |
|
STATUS_ERR_INVALID_ARG |
The supplied read length was invalid |