10.6.3.2.5 Function nvm_erase_row()
Erases a row in the NVM memory space.
enum status_code nvm_erase_row( const uint32_t row_address)
Erases a given row in the NVM memory region.
| Data direction | Parameter name | Description |
|---|---|---|
|
[in] |
row_address |
Address of the row to erase |
Returns
Status of the NVM row erase attempt.
| Return value | Description |
|---|---|
|
STATUS_OK |
Requested NVM memory row was successfully erased |
|
STATUS_BUSY |
NVM controller was busy when the operation was attempted |
|
STATUS_ERR_BAD_ADDRESS |
The requested row address was outside the acceptable range of the NVM memory region or not aligned to the start of a row |