10.6.3.2.6 Function nvm_execute_command()
Executes a command on the NVM controller.
enum status_code nvm_execute_command( const enum nvm_command command, const uint32_t address, const uint32_t parameter)
Executes an asynchronous command on the NVM controller, to perform a requested action such as a NVM page read or write operation.
| Data direction | Parameter name | Description |
|---|---|---|
|
[in] |
command |
Command to issue to the NVM controller |
|
[in] |
address |
Address to pass to the NVM controller in NVM memory space |
|
[in] |
parameter |
Parameter to pass to the NVM controller, not used for this driver |
Returns
Status of the attempt to execute a command.
| Return value | Description |
|---|---|
|
STATUS_OK |
If the command was accepted and execution is now in progress |
|
STATUS_BUSY |
If the NVM controller was already busy executing a command when the new command was issued |
|
STATUS_ERR_IO |
If the command was invalid due to memory or security locking |
|
STATUS_ERR_INVALID_ARG |
If the given command was invalid or unsupported |
|
STATUS_ERR_BAD_ADDRESS |
If the given address was invalid |