14.7.3.2.1 Function rtc_count_set_count()
Set the current count value to desired value.
enum status_code rtc_count_set_count( struct rtc_module *const module, const uint32_t count_value)
Sets the value of the counter to the specified value.
| Data direction | Parameter name | Description |
|---|---|---|
|
[in, out] |
module |
Pointer to the software instance struct |
|
[in] |
count_value |
The value to be set in count register |
Returns
Status of setting the register.
| Return value | Description |
|---|---|
|
STATUS_OK |
If everything was executed correctly |
|
STATUS_ERR_INVALID_ARG |
If invalid argument(s) were provided |