15.4.2.3.1 Setup for Using PLL with the Primary Oscillator (POSC)
The following process is used to set up the PLL to operate the device at 200 MIPS with a 10 MHz external crystal:
- Set the configuration for the POSC to HS mode using POSCMD[1:0] bits in the OSCCFG register.
- Setting up divider settings: to execute instructions at 200 MHz, a PLL output frequency
of 200 MHz will be required. To set up the PLL and meet the requirements of the PLL,
follow these steps:
- Select the PLL prescaler.
- Select a PLL prescaler value of N1 = 1
- FPLLI = 10 MHz
- FPFD = 10 MHz(1/N1) = 10 MHz(1) = 10 MHz
- Select the feedback divider to meet the VCO output frequency requirement, as well
as achieve the desired FVCO frequency.
- Select a feedback divider value of M = 100
- FVCO = FPLLI x (M/N1) = 10 MHz x (100/1) = 1 GHz
- Select values for the first and second PLL postscalers to achieve the required
FPLLO frequency.
- Select values for the first and second postscalers of N2 = 5 and N3 = 1
- FPLL FOUT/FPLLO = FVCO/(N2 x N3) = 1 GHz/5 = 200 MHz
- Enable the PLL Input and Feedback Divider update by setting PLLSWEN bit in the PLLxCON register. Enable the PLL Output Divider update by setting FOUTSWEN bit in the PLLxCON register.
- Select clock source by setting NOSC[3:0] bits in the PLLxCON register to Primary (3).
- Enable clock switching by setting OSWEN bit in the PLLxCON register.
- Select the PLL prescaler.
- Writing PLLxCON (can be done in one PLLxCON write):
- Enable the PLL input and Feedback Divider update by setting PLLSWEN bit in the PLLxCON register. Enable the PLL Output Divider update by setting FOUTSWEN bit in the PLLxCON register.
- Select clock source by setting NOSC[3:0] bits in the PLLxCON register to Primary (3).
- Enable clock switching by setting OSWEN bit in the PLLxCON register.
Note: PLL1CON writes written out for clarity, These writes
can be achieved in a single PLL1CON write.
Code Example for Using PLL with the Primary Oscillator (POSC)
// code example for 200MIPS PLL clock using 10MHz crystal primary oscillator
//set crystal configuration using configuration register
OSCCFGbits.POSCMD = 2; //set desired Primary oscillator mode
// 0b00 : EC mode
// 0b10 : HS mode
// 0b01 : XT mode
// 0b11 : Disabled
//Enable PLL clock generator
PLL1CONbits.ON = 1;
PLL1CONbits.OE = 1;
//configure backup oscillator in case of failure
PLL1CONbits.BOSC = 2; //select BFRC backup clock source:
PLL1CONbits.FSCMEN = 1; //enable fail safe
//configure PLL values
PLL1DIVbits.PLLFBDIV = 100; //Feedback Divider
PLL1DIVbits.PLLPRE = 1; //Reference Clock Divider
PLL1DIVbits.POSTDIV1 = 5; //Post Divider #1
PLL1DIVbits.POSTDIV2 = 1; //Post Divider #2
// PLL Fout = Fin*FBDIV / (PLLPRE * POSTDIV1 * POSTDIV2)
// PLL Fout = 10M*100/(1*5*1) =200MHz
//Enable PLL Input and Feedback Divider update
PLL1CONbits.PLLSWEN = 1;
while (PLL1CONbits.PLLSWEN == 1);
//Enable PLL Output Divider update
PLL1CONbits.FOUTSWEN = 1;
while (PLL1CONbits.FOUTSWEN);
//select clock switching clock source
PLL1CONbits.NOSC = 3; //select POSC clock source
//[1] = FRC - Internal 8 MHz RC oscillator
//[2] = BFRC - Internal Backup 8 MHz RC oscillator
//[3] = POSC - Primary crystal oscillator (4-32 MHz)
//[9] = REFI1 - user definable clock source
//[10] = REFI2 - user definable clock source
PLL1CONbits.OSWEN = 1; //enable clock switching
while (PLL1CONbits.OSWEN); //wait for switching(hardware clear)
while(!OSCCTRLbits.PLL1RDY); //wait for clock to be ready