15.4.1.2 Setup for Using Clock Generator with 8 MHz Internal FRC
The following process is used to set up the CLKGEN1 to operate the device with an 8 MHz Internal FRC:
- To set up the fail-safe for the
clock generator, follow these steps:
- Select the backup clock source by selecting the BOSC bits in CLKxCON register.
- Enable fail-safe clock failure by setting the FSCMEN bit in CLKxCON register.
- Enable ClkFailInterrupt to generate an interrupt during clock failure.
- To switch to a new oscillator for
the clock generator, follow these steps:
- Select clock source to switch by writing to NOSC bits in the CLKxCON register.
- Enable switching by writing to the OSWEN bit in the CLKxCON register.
- To further divide the clock out of
the clock generator using CLKxDIV, follow these steps:
- Set the integer divide factor bit setting INTDIV bits in the CLKxDIV register.
- Set the fractional divide factor bit setting FRACDIV bits in the CLKxDIV register. FRACDIV will not work if INTDIV is configured to 0.
- Set the DIVSWEN bit in the CLKxCON register to enable divide factors to get updated.
- Enable the clock generator (if not enabled by default) by setting the ON bit in CLKxCON register.
Code Example for Clock Generator 1 Switching to FRC
//enable clock generator
CLK1CONbits.ON = 1;
CLK1CONbits.OE = 1;
//configure backup oscillator in case of failure
CLK1CONbits.BOSC = 2; //BFRC
//select backup clock source:
//[1] = FRC - Internal 8 MHz RC oscillator
//[2] = BFRC - Internal Backup 8 MHz RC oscillator
//[3] = POSC - Primary crystal oscillator (4-32 MHz)
//[4] = LPRC
//[5] = PLL1 Fout output
//[6] = PLL2 Fout output
//[7] = PLL1 VCO FracDiv output
//[8] = PLL2 VCO FracDiv output
//[9] = REFI1 - user definable clock source
//[10] = REFI2 - user definable clock source
CLK1CONbits.FSCMEN = 1; //enable fail safe
//configure clock divide
CLK1DIVbits.INTDIV = 1; //integer divide factor
CLK1DIVbits.FRACDIV = 0x0080; //fractional divide factor
CLK1CONbits.DIVSWEN = 1; //enable divide factors to get updated
while (CLK1CONbits.DIVSWEN); //hardware cleared
// Fdiv = Fin / 2*(INTDIV+(FRCDIV/512))
//enable clock switching
CLK1CONbits.NOSC = 1 ; //select clock source
//[1] = FRC - Internal 8 MHz RC oscillator
//[2] = BFRC - Internal Backup 8 MHz RC oscillator
//[3] = POSC - Primary crystal oscillator (4-32 MHz)
//[4] = LPRC
//[5] = PLL1 Fout output
//[6] = PLL2 Fout output
//[7] = PLL1 VCO FracDiv output
//[8] = PLL2 VCO FracDiv output
//[9] = REFI1 - user definable clock source
//[10] = REFI2 - user definable clock source
CLK1CONbits.OSWEN = 1; //enable clock switching
while (CLK1CONbits.OSWEN); //wait for switching(hardware clear))
IFS0bits.CLKFAILIF = 0; // enable clock failure interrupt
IEC0bits.CLKFAILIE = 1;
}