2.109.12 SENTx_Transmit Function
C
/* x refers to the instance number */
void SENTx_Transmit(const SENT_DATA_TRANSMIT *sentData)
Summary
Transmits the data to the receiver of the SENT Peripheral when it acts like a transmitter.
Description
This function is responsible for transmitting data from the SENT peripheral. The function will transmit the desired data.
Precondition
The SENTx peripheral must have been initialized using the SENTx_Initialize API. The peripheral should be enabled using the SENTx_Enable() API.
Parameters
| Param | Description |
| sentData | a structure data type SENT_DATA_TRANSMIT Struct |
Returns
None.
Example
struct SENT_DATA_TRANSMIT data; data.data1 = 0x01; data.data2 = 0x02; data.data3 = 0x03; data.status = 0x00; SENT1_Initialize(); while(!SENT1_IsTransmissionComplete()); SENT1_Transmit(&data);
Remarks
None.