2.109.10 SENTx_ReceiveErrorGet Function
C
/* x refers to the instance number */
SENT_ERROR_CODE SENTx_ReceiveErrorGet(void)
Summary
Returns the type of reception error when the SENT Peripheral acts as a receiver.
Description
This function returns the most recent error code that was recorded during reception.
Precondition
Ensure that the SENT instance is properly initialized and configured before calling this function..
Parameters
None.
Returns
Returns the SENTx module reception error SENT_ERROR_CODE Enum
Example
SENT_ERROR_CODE errorCode = SENT2_ReceiveErrorGet();
if (errorCode != NO_ERROR) {
/*Handle the error accordingly*/
}
Remarks
None.