2.32.5 DMAC_ChannelPatternMatchSetup Function

C

The prototype of this function varies based on device family. Refer to the generated header file for the actual prototype to be used.

void DMAC_ChannelPatternMatchSetup(DMAC_CHANNEL channel, uint8_t patternMatchData);
void DMAC_ChannelPatternMatchSetup(DMAC_CHANNEL channel, DMAC_DATA_PATTERN_SIZE patternSize, uint16_t patternMatchData);

Summary

Sets up DMA channel for pattern matching

Description

This function sets up a DMA channel for pattern matching. while transferring the data via DMA, if data chunk is matched with the given data, then DMA transfer stops. This feature is useful in applications where a variable data size is required and eases the set up of the DMA channel. UART is a good example of where this can be effectively used.

Parameters

Parameters of this function varies based on device family. Refer to the one which is applicable for the device being used. | Param | Description | |:----- |:----------- | | DMAC_CHANNEL channel | the particular channel to be setup for pattern matching | | patternMatchData | 8 bit data to be matched

ParamDescription
DMAC_CHANNEL channelthe particular channel to be setup for pattern matching
patternSizeselects pattern data size
patternMatchDatapattern data to be matched

Returns

None.

Example

Example of this function varies based on device family. Refer to the one which is applicable for the device being used.

DMAC_ChannelPatternMatchSetup (DMAC_CHANNEL_0, 0x55);
DMAC_ChannelPatternMatchSetup (DMAC_CHANNEL_0, DMAC_DATA_PATTERN_SIZE_1_BYTE, 0x55);