4.3.1.6.2 Plot Cursors

A vertical cursor can be used in a similar manner to the plot marker, except that the cursor does not follow mouse movements; it must be dragged to a position and it will not move until dragged again. To add one or more cursors to the display, click on the top of the graph and click on the Add vertical cursor icon . “Inspect Values” will then display cursor values in place of marker values (see figure).

Figure 4-22. Vertical Cursor A
Table 4-5. Inspect Values Display
Jump to cursor. The cursor will be centered on the graph and scrolling is paused. If the cursor has scrolled away with the plot, jump to its location.
Reposition the cursor to the center of the graph. Hold the shift key when repositioning to move all cursors the same amount.
Delete the cursor.
A, B, C, etc.The letter number of the cursor.
Time ValuesFor each cursor, the value where the cursor intersects the time axis is displayed (timestamp).

For two or more cursors, a time difference (delta) is displayed, with the leftmost cursor as reference.

Frequency ValueFor two or more cursors, hover over the time values to see a frequency value, with the leftmost cursor as reference.
Data ValuesFor each cursor, the value where the cursor intersects the data plot is displayed at the current zoom level. If there is more than one plot, a color bar corresponding to the plot color will signify the associated data value. For two or more cursors, a data difference (delta) is displayed, with the leftmost cursor as reference.

Cursors behave differently in Run Mode vs Stopped Mode. When in Run mode, the cursor values will update every 100 ms. This is to give an idea of data fluctuations and isn't intended for use where accurate data analysis is needed. See Stopped Mode or data logging for applications where better accuracy is desired.

Off screen cursors will show n/a during Run Mode, but will update when Stop is clicked.

For Stopped Mode, off screen cursors will show data values as long as the corresponding data hasn't been discarded.

Use Two Cursors for Bandwidth

Two vertical cursors can be used to determine bandwidth. Using the time delta, for example in the figure below, the time difference between the position of A and of B is 660 ms. Therefore the bandwidth is 660 ms / 4 cycles ≅ 165 ms/cycle.

Note: As there may be variation between cycles, it is usually best to measure time over several cycles to provide an average value.
Figure 4-23. Add Two Vertical Cursors - Bandwidth

Use Three Cursors for Duty Cycle

Adding a third cursor allows you to calculate the duty cycle. If A-C is the period, then A-B is shown as a percentage of that (50.5%).

Figure 4-24. Add Three Vertical Cursors - Duty Cycle

Additional cursors may be added to the graph.