5.2.6 Set Enter Command Character

Format: S$,<char>

This command sets the Command mode character, where <char> is a single character in the three character pattern. This setting enables the user to change the default character to enter Command mode ($$$) to another character string. For restoring the factory defaults, configure the enter command character as $$$.

ItemFirmware Version 1.0 and LaterDescription
Default:$
Example:S$,#Set ### as string to enter Command mode
Response:AOKSuccess
ErrSyntax error or invalid parameter
Note: The PDS stores the parameter, and the user can bring it into immediate effect without a reboot.