5.2.25 Set HCI Determination or Set HCI

Table 5-15. Format
Firmware Version 1.0Firmware Version 1.2 and Later
SH,<0,1>

SCHI,<0,1>

Note: All firmware version 1.0 syntax remains valid in version 1.2 and later.
This command is used to enable/disable the determining scheme to enter the HCI mode:
  • 1: Enable HCI mode determining scheme
  • 0: Disable HCI mode determining scheme

The determining scheme is to check the first command format to judge if the RNBD350 module is in HCI mode or RN application after reboot. When the RNBD350 module enters HCI mode, it will be recorded into PDS and invalidate the determining scheme. The GH or GCHI command will navigate to the Get_Configuration.

ItemFirmware Version 1.0 and LaterDescription
Example:SH,1Enable HCI mode determining scheme
Response:AOKSuccess
ErrSyntax error or invalid parameter
Note:
  • The command is supported in RNBD350 v1.1 and later.
  • The parameter of SH command is stored in PDS.
ItemFirmware Version 1.2 and LaterDescription
Example:SHCI,1Enable HCI mode determining scheme
Response:AOKSuccess
ErrSyntax error or invalid parameter
Note:
  • The command is supported in RNBD350 v1.1 and later.
  • The parameter of SHCI command is stored in PDS.